FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
02-09-2022 08:41 AM
Hello,
When we export the real-data in the ctrlX IO it appears the following errors exporting the SAFEX,
I don't really know if it is because of this error but then in the PLC app we cannot find the .xml of the SAFEX,
We are using the last version of the ctrlX IO and PLC (1.12) and we have inserted the xml of the device,
Is there a way to import the xml of the SAFEX to the PLC?
Thanks,
Solved! Go to Solution.
03-15-2022 10:12 AM - edited 03-15-2022 12:00 PM
It has been 5 weeks and still no one has replied to this topic...
We are in the middle of an important project so it would be great if anyone could give us an answer related to this,
Thanks,
03-15-2022 12:25 PM - edited 03-15-2022 03:55 PM
Hello,
1. the first screenshot is a well known behaviour - it is not a feature its a bug(314259) in the ctrlX IO Engineering. Development is working on it - solving date is not planned yet.
2. The ESI File for the ctrlX SAFETY is not delivered with the ctrlX WORKS Package.
You have to collect it in the Collaboration room: SAFEX-C.1x ESI-File
Install it into your project into the IO-Engineering.
We think you just installed the ESI in the IO-Engineering. For the PLC Engineering yoiu do not need the ESI file.
When the configuration is finnished in the ctrlX IO-Engineering, you have to transfer the configuration from the IO-Engineering to the control.
Afterwards you can fetch the IO-configuration in the PLC-Engineering with the steps:
Then you will see the FSoE and the functional IO from the ctrlX SAFETY in the PLC project.
03-15-2022 07:43 PM
Sorry Eric,
for a long time we had no traffic. We did not look so intensively into this forum. We'll track this now much more tight.
Best regards
03-15-2022 07:55 PM
Just to avoid further questions.
At the moment the ctrlX SAFETY development is not completely synched with the RM sequence for the rest of ctrlX AUTOMATION.
This will change in the future:
The target date for that integration into ctrlX WORKS is not yet defined.
03-16-2022 04:14 PM - edited 03-16-2022 04:14 PM
Hello ChrM and Scheurer_F,
We have tried the .xml and the problem still persists,
We can see the SAFEX in the ctrlX IO Software, the problem is that in the ctrlX PLC it does not appear in the "DataLayer_Realtime" and, as a consequence, we cannot communicate between the ctrlX Core and the SAFEX,
03-17-2022 01:59 PM
Same here... I can only get to work until the point, where the C12 is present in the EtherCAT configuration on the coreX but remains in the Pre-OP state with a 0x001E Invalid Input Configuartion Error:
The section, which should include the description for using the C12 with coreX in the installation manual for the C.1x only refers to a document with the description "ctrlX AUTOMATION DOK-XSAFE*-SAFEX-C.1XC-APxx-DE-P". Unfortunatly I am not able to find this very document...
Is there any solution in sight?
03-17-2022 03:53 PM
03-18-2022 10:16 AM
Thanks for your reply! I tried to configure the topology with the I/O Engineering tool. Here you file unfortunately doesn't work here. It just tells me, that the file doe not contain anything, that could be imported.
03-18-2022 03:10 PM - edited 03-21-2022 03:03 PM
My understanding is that SAFEX-C12 has been added to the ctrlX IO project\configuration then transfered to the CORE. After, the IO configuration should be imported to PLC Engineering by reading online from CORE. This reading online from the CORE is not working or reading the SAFEX-C12. If this is the case the attached files and PDF will help guide you to import the SAFEX-C12 from a file instead of online from CORE.
HTH
03-18-2022 08:32 PM
Thank you very much, ctrlXProgrammatore,
for giving additional assistance to ericvergara.
I honestly admit, that there are a few obstacles in the process of integrating SAFEX-C.1x into an EtherCAT configuration:
Best regards
Your ctrlX SAFETY Team
04-07-2022 10:08 AM
Hello ctrlxProgrammatore and Scheurer_F,
Sorry for the delay, we have now tried with the solution that ctrlXProgrammatore gave us and it worked!
We can now communicate between the ctrlX Core and the SAFEX via the Data Layer,
Thanks for the help!
09-20-2022 10:51 AM
03-09-2023 02:48 PM
Hello,
sorry to drag this old topic out of the dirt:
I'm currently trying to configure my I/O engineering and I have a Safex-C.15 controller. And it is not in my parts list to select.
It is mentioned here, that it is not part of the normal ctrlX Works installation. But the provided links, where you could download an ESI-file, are not working anymore. And I don't find alternatives.
Could anyone provide me with a link, where I can get the ESI-File for SafeX-C15?
Thanks in advance!
05-12-2023 03:32 PM
Hi, I need this ESI File:
......2. The ESI File for the ctrlX SAFETY is not delivered with the ctrlX WORKS Package.
......You have to collect it in the Collaboration room: SAFEX-C.1x ESI-File
for the connection to a Beckhoff PLC together with ControlPlus.
The AML Export will have this file to finish the RUN in the ControlPlus Environment.
The Link (appears as missing link to "33358678") is not working.
It's honestly a nightmare that it is so complicated to get ESI Files (in general) from BoschRexroth.
Frank
05-15-2023 02:06 AM
Hello @FrankSwierza1 and @TBauer , sorry for any inconvenience, we are working on the integration into ctrlX WORKS.
the way to the collaboration room is described here. Yes indeed, our whole download area has been running through some changes and some of the links were discontinued.
Once again sorry for the trouble finding the download area in Collaboration Room!
Best regards
Your ctrlX SAFETY team