FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important
information on the platform change.
01-05-2022 10:41 PM - edited 01-07-2022 01:17 PM
I am running MC_Home command. If the Position input is 0.0 then the command runs and completes correctly. If the Position is non zero then the command goes into error. I am using motion app 1.12. We are using drives with MPB20 firmware.
Solved! Go to Solution.
01-06-2022 08:48 PM
I see the same problem also. Here are the error codes from MC_Home and ctrlX diagnostics. I could not find anything in the online help about these codes. We can tell that 0 is succesfully being written to S-0-0052 when 0 is the value for Position. However, as Craig mentioned, any other value causes a severe error.
Thanks,
Brian
01-10-2022 10:50 AM
Hello,
with the search function I also did not find the error code 090F2040, but with a look at the error codes of ctrlX MOTION "09" I found also 090F2040.
01-13-2022 12:16 AM
The solution was that the Position input of MC_Home must within the range of the software travel limits (S-0-0049, S-0-0050), even if software travel limits are not enabled.
05-11-2022 08:20 AM
Hello,
this bug was fixed with RM21.11.2.
Best regards,
Michael