FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
08-16-2022 04:44 AM
Hello,
Since updating to 1.16 I now see a yellow warning state of the light pipe due to low battery. I think I have only seen red, blue or green on X3 before this. The warning is persistent. I replaced the battery but still get the low battery warning, presumably because I have the old battery holder preventing good contacts. The real fix is to get a new battery holder, but until I receive this (and as a general question) is it possible to suppress/ignore warnings so the LED can be green if no error present?
Best regards,
Brian
Solved! Go to Solution.
08-16-2022 04:01 PM
I had the same question and currently this is not possible. I asked for a function to acknowledge the warning which would stop the yellow blinking. Since this is not a security warning this could be an additional function
08-17-2022 03:28 AM
Hello,
I had the same issue with my ctrlX drive demo unit too, after upgrading to version 1.16 the ctrlX flashes yellow and prompting me to change battery. After i changed the battery it still flashes yellow and prompting me that my battery level is low.
Warmest regards,
08-17-2022 02:17 PM
05-23-2023 04:59 PM
Brian,
I'm not sure if this is something new in V1.20, it is possible to disable the warning by setting the hide-diagnosis value to true in the data layer.