cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Suppression of warning yellow LED on ctrlX CORE X3

Suppression of warning yellow LED on ctrlX CORE X3

bschmidt
New Contributor

Hello,

Since updating to 1.16 I now see a yellow warning state of the light pipe due to low battery. I think I have only seen red, blue or green on X3 before this. The warning is persistent. I replaced the battery but still get the low battery warning, presumably because I have the old battery holder preventing good contacts. The real fix is to get a new battery holder, but until I receive this (and as a general question) is it possible to suppress/ignore warnings so the LED can be green if no error present?

Best regards,

Brian

4 REPLIES 4

Marc_Smaak
Long-established Member

I had the same question and currently this is not possible. I asked for a function to acknowledge the warning which would stop the yellow blinking. Since this is not a security warning this could be an additional function

Open
New Contributor

Hello,

I had the same issue with my ctrlX drive demo unit too, after upgrading to version 1.16 the ctrlX flashes yellow and prompting me to change battery. After i changed the battery it still flashes yellow and prompting me that my battery level is low. 

Warmest regards,

Michael_A
Long-established Member
Is it possible that you use a system/root user on your control? If yes, this will be signalled too with a yellow warning of the light pipe

joeG
Established Member

Brian,

I'm not sure if this is something new in V1.20, it is possible to disable the warning by setting the hide-diagnosis value to true in the data layer.

joeG_0-1684853839341.png

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist