08-04-2022 04:04 AM
Hi everyone👋,
I'm here for asking , when i try to install node-red aedes broker on ctrlX node-red but i get the this error.
the error is shown on the picture below
we have already try uninstall and install again but it's doesn't work, could it be the certificate issue?
thank you and appreciate your guidance if you are able to solve this issue! 😊
Solved! Go to Solution.
08-04-2022 07:35 PM
Is the real time clock in your ctrlX set to the correct time/date?
08-05-2022 06:33 PM
Hi Joex,
yes we already change the time , but still have a same error.
By the way thanks for responding. 😊
08-08-2022 08:11 AM
In the ctrlX CORE - Node-RED App we are using as fixed setting "NODE_TLS_REJECT_UNAUTH*". This is needed for our communication because the ctrlX CORE has a self signed certificate. Perhaps the node-red-contrib-aedes cannot work with this. We are going to check this.
In our tests we used a mosquitto broker up to now and it worked quite fine. You could for example use the the Cedalo - Eclipse Mosquitto MQTT Broker as installable app.
08-11-2022 06:00 AM
Thanks for your idea,
but i can't install the MQTT as wel, i have the error when install.
the error shown on the picture below
08-11-2022 07:54 AM
Like mentioned in the error code the app you try to install is not certified by rexroth so you have to allow installation from unknown sources.
ctrlX CORE app installation settingsctrlX CORE app installation settings
08-11-2022 08:26 AM
Hi,
@CodeShepherdyes you are right. That's what the error says and how you can work around this error.
But the Cedalo - Mosquitto MQTT Broker App is signed by Bosch Rexroth and if you get the version from the here this should not be necessary.
Best regards,
Nick
08-16-2022 04:08 AM
Thanks for reply,
May i ask how to enable or disable the certificate?
so that maybe can solve the error.
08-17-2022 07:29 AM
You cannot enable or disable the certification in an app. Apps from our official store are always certified.
What you can do, like mentioned in my post above, to tel the ctrlX CORE to allow the installation from unknown source. That means apps without an certificate.