Hello there It is possible to use ctrlX HMI apps to create a pipeline animation that replicates the flow of water by using replacing dots. This can be placed into effect by producing a unique animation that represents the flow of water through the pipeline. When interacting the direction and speed of the flow; fluid characteristics such as a flowing line and moving dots might be used. You can add this animation into your user interface to give real time feedback on the operational state of the pipeline due to the flexibility of ctrlX HMI.
... View more