Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Light Curtain Muting with ICS Function Block

Light Curtain Muting with ICS Function Block

GoHawks
Established Member

Hello,

 

We are trying to mute a light curtain with the ICS function in CtrlX Safety Engineering, but the function block is only availible with a Beckhoff Remote IO module. In our application, the light curtains will be wired directly to the C15.

Please advise.

7 REPLIES 7

Dias
Community Moderator
Community Moderator

Hello,

I need more information.

Which Beckhof module you use that you get an ICS-FB. Please append your example program.

GoHawks
Established Member

Hi Dias,

Thank you for looking into this.

Below you can see that if I connect a light curtain to the EP1908-002 Remote IO block, I can see the option to select a ICS function block:

GoHawks_0-1673453778941.png

GoHawks_1-1673453924672.png

But if i connect a light curtain straight to the C15, it no longer is available to select:

GoHawks_2-1673454016332.png

GoHawks_3-1673454042533.png

In my application, we MUST connect the light curtains to the C15.

Thank you in advance!

FYI, using the following CtrlX Safety Version:

GoHawks_0-1673454311766.png

 

 

Dias
Community Moderator
Community Moderator

Hello GoHawks,

all these objects are FSoE-Objects. That means if you put an object like this into the Terminal Scheme:

Dias_0-1673507882041.png

You can program it one time:

Dias_1-1673508149281.png

For using FSoE-Slave-Objects you need a running Ethercat with e.g. ctrlX CORE as an Ethercat-Master and the ctrlX CORE PLC must copy the FSoE Datas from/to FSoE-Master (ctrlX SAFETY) from/to FSoE-Slave (e.g. Beckhof device)

In your third screenshot I missed in the Terminal Scheme the Beckhof FSoE-Slave object. Why? It was configured before?

 

GoHawks
Established Member

Hi Dias,

Perhaps I confused this topic a little. I need muting functions for light curtains going to CtrlX Safety C15. I presumed the ICS function block was the correct function block to use because it mentioned muting in the documentation. It sounds like this can only be used with FSOE devices...

Regardless, I am looking for ways to mute a light curtain, simliar to some of the Bosch SafeLogic Compact and SafeLogic safety PLCs.

GoHawks_0-1673642146810.png

GoHawks_1-1673642209707.png

Any advice would be greatly appreciated.

GoHawks!

Hello @GoHawks and @Dias ,

as far as I understand the question and read the documention

ICS Online DocumentationICS Online Documentation

the ICS function works like this:

  • The input to be muted is selected in the properties dialog of the ICS block
  • while the muting activation is done by the activation input of the block.

Is this the direction you think @GoHawks ?

Your ctrlX SAFETY team

@GoHawks and @Dias ,

I tried to use the ICS function block. Actually it can only be applied to the EP1908.

ICS Muting Test ScenarioICS Muting Test Scenario.

I'll open an issue for this.

Your ctrlX SAFETY team

 

@GoHawks and @Dias ,

for the time being the ICS Input element muting is not available for IO on the SAFEX-C.1x.

A short term solution or workaround has to be addressed in the application talks.

For the later a clear specification of the expected behavior has to be provided, e.g. to generate a work-around:

  • What alarms shall be muted?
  • Is it just a bypass that shall mute the activation of the light curtain?
  • If it is a bypass, are there any other limitations to be added? Min/Max time, etc.
  • What inputs and outputs shall the workaround block have?
  • What input/output behavior is expected as truth table and in time dimension?

@Dias : Any proposals for a workaround?

Best regards

Your ctrlX SAFETY team

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist