07-29-2021 03:51 PM - edited 07-29-2021 03:58 PM
Hello,
Just wanted to show something i found out myself.
I had this error when switching from config to running mode:
Solution:
Create a task for motion manually.
EDIT: maybe someone can confirm if this is the intended procedure from now on.
Cheers
Solved! Go to Solution.
08-03-2021 11:22 AM - edited 08-03-2021 11:31 AM
It is a known topic because of an update from RM21.03 (v1.8) to RM21.07 (v1.10) and using the old AppData (active configuration).
See also this topic.
08-05-2021 07:24 AM
08-05-2021 08:27 AM
Your picture shows that the ctrlXAutomation task was set to a non realtime cpu core (Nr 1). See my working settings below.
08-05-2021 09:56 AM
thanks a lot, I am clear now ~