cancel
Showing results for 
Search instead for 
Did you mean: 

MB_CamIn synchronizing to wrong position after power cycle

MB_CamIn synchronizing to wrong position after power cycle

joeG
Established Member

I am using the MB_CamIn Function block with 8 axes that are need a 45° master offset from each other (0°, 45°, 90°, ..., 315°). The first time after power up when I put the master offset in the DynOffsets.Master.Position input it fist goes to the 0° offset position, then goes to the correct position. If I put the offset into the CamIn.MasterOffset it behaves as I would expect, but that input does not appear to be cyclically read. I would expect both master offsets to behave the same when synchronizing.

Here is a picture of what I see and the cam I am testing with.

I am using version 3.2.0 of the motion app.

first_sync.png

2 REPLIES 2

NormalOne
Established Member

This happened only after "first time after power up", isn't it?
I could reproduce it and I addressed the topic internally. 

joeG
Established Member

Correct, I only see it the first time after power up.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist