FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
3 weeks ago
I am using the MB_CamIn Function block with 8 axes that are need a 45° master offset from each other (0°, 45°, 90°, ..., 315°). The first time after power up when I put the master offset in the DynOffsets.Master.Position input it fist goes to the 0° offset position, then goes to the correct position. If I put the offset into the CamIn.MasterOffset it behaves as I would expect, but that input does not appear to be cyclically read. I would expect both master offsets to behave the same when synchronizing.
Here is a picture of what I see and the cam I am testing with.
I am using version 3.2.0 of the motion app.
2 weeks ago
This happened only after "first time after power up", isn't it?
I could reproduce it and I addressed the topic internally.
2 weeks ago
Correct, I only see it the first time after power up.