01-23-2024 03:10 PM
Hello,
Since updating my demo to 2.04, I am seeing that the Core crashes when I download my ctrlX IO Engineering configuration. It is related to the Motion state. If the Motion is in Running state when I do the EtherCAT download, the crash happens. If I first go to Configuration Mode with Motion and then download EtherCAT I have no problems. In the past this was handled automatically, or at least did not cause a crash. I see it with both of my X3’s, even with a fresh system image and only the EtherCAT and Motion apps installed.
Basic sequence starting from fresh image and EtherCAT and Motion apps installed:
At that point I have to reboot the Core. Sometimes it takes 2 reboots to make it happy.
Best regards,
Brian
02-01-2024 03:13 PM
As we are not able to reproduce your error, could you switch on motion and EtherCat traces and create a system report in error case? See how to.
03-05-2024 05:48 PM
Hello ,
I had the same situation. The only way to avoid this for me is to put the Machine in Setup and make sure the EtherCat master is in INI. I also stopped the PLC
09-12-2024 08:31 AM
Are there any news? Is this still an issue?