Downloading IO Configuration with Motion in Running causes apps to crash

Downloading IO Configuration with Motion in Running causes apps to crash

bschmidt
New Contributor

Hello,

Since updating my demo to 2.04, I am seeing that the Core crashes when I download my ctrlX IO Engineering configuration. It is related to the Motion state. If the Motion is in Running state when I do the EtherCAT download, the crash happens. If I first go to Configuration Mode with Motion and then download EtherCAT I have no problems. In the past this was handled automatically, or at least did not cause a crash. I see it with both of my X3’s, even with a fresh system image and only the EtherCAT and Motion apps installed.

Basic sequence starting from fresh image and EtherCAT and Motion apps installed:

  • Add EtherCAT master instance
  • Make new IO Engineering project, add drive to project
  • Download IO Engineering project, no problems, EtherCAT goes to OP
  • Add Axis Profile in Motion app. Map minimum data to drive added above.
  • Switch Motion from Configuration to Running, no problem
  • Download IO Engineering project again: Core crashes. See screenshots below.

At that point I have to reboot the Core. Sometimes it takes 2 reboots to make it happy. 

bschmidt_0-1706018571938.png

bschmidt_1-1706018571948.png

bschmidt_2-1706018571953.png

bschmidt_3-1706018571965.png

Best regards,

Brian

 

3 REPLIES 3

CodeShepherd
Community Moderator
Community Moderator

As we are not able to reproduce your error, could you switch on motion and EtherCat traces and create a system report in error case? See how to.

YUL725
Long-established Member

Hello ,

I had the same situation. The only way to avoid this for me is to put the Machine in Setup and make sure the EtherCat master is in INI. I also stopped the PLC

CodeShepherd
Community Moderator
Community Moderator

Are there any news? Is this still an issue?

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist