cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Import I/O configuration offline

Import I/O configuration offline

rku
Established Member

Is it possible to import an I/O configuration made with ctrlX I/O Engineering to ctrlX PLC Engineering not being online in a real or virtual Core? There is this "Offline from file..." option in PLC Engineering. How is such a file created?

rku_0-1653299113662.png

 

6 REPLIES 6

CodeWasi
New Contributor

Hello,

in case the configuration is already on the control -> download available under:

CodeWasi_1-1653393958041.png

without the data being available on the ctrlX. Edit the ctrlXIOEng and download the config via "Saving Ethercat configuration...":

exporting command of EtherCat masterexporting command of EtherCat master

if not listed yet, see "Tools" -> "Customize":

export IO configuration settingexport IO configuration setting

Finally the data can be added "offline".

PLC Engineering import EtherCat configuration from filePLC Engineering import EtherCat configuration from file

OK?

Bye

rku
Established Member

I don't have that "Generate EtherCAT XML" option.

rku_0-1653899169733.png

rku_2-1653899244632.png

 

 

CodeShepherd
Community Moderator
Community Moderator

You have add it to your visible menu. See post above.

rku
Established Member

Yes, I got that. But I can't find it in the Tools - Customize menu. As you can see from my post, the menu contents are different to that of CodeWasi.

CodeShepherd
Community Moderator
Community Moderator

I updated the screenshot to make it clearer. The entry is missing in general and you have to add it. Please see post above.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist