05-23-2022 11:49 AM
Is it possible to import an I/O configuration made with ctrlX I/O Engineering to ctrlX PLC Engineering not being online in a real or virtual Core? There is this "Offline from file..." option in PLC Engineering. How is such a file created?
Solved! Go to Solution.
05-24-2022
02:13 PM
- last edited
4 weeks ago
by
CodeShepherd
Hello,
EDIT: There is an how to available: "Import EtherCAT IO realtime data offline into ctrlX PLC Engineering"
in case the configuration is already on the control -> download available under:
without the data being available on the ctrlX. Edit the ctrlXIOEng and download the config via "Saving Ethercat configuration...":
exporting command of EtherCat master
if not listed yet, see "Tools" -> "Customize":
export IO configuration setting
Finally the data can be added "offline".
PLC Engineering import EtherCat configuration from file
OK?
Bye
05-30-2022 10:27 AM
I don't have that "Generate EtherCAT XML" option.
05-30-2022 11:31 AM
You have add it to your visible menu. See post above.
05-30-2022 11:44 AM
Yes, I got that. But I can't find it in the Tools - Customize menu. As you can see from my post, the menu contents are different to that of CodeWasi.
05-30-2022 11:54 AM
I updated the screenshot to make it clearer. The entry is missing in general and you have to add it. Please see post above.
02-20-2023 05:52 PM