FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
05-12-2020 11:04 AM
Which parameter is for activation of the simulation mode (because there is no menu für ctrlX Drive) ? |
Solved! Go to Solution.
05-13-2020 05:14 PM
Axis simulation like in the past is already possible.
Additional information: In the very moment both IndraWorks Ds 15V06 and ctrlX DRIVE Engineering don´t support the offline simulation of a drive no matter if you create it from an existing parameter file or configure it.
The only thing possible in the very moment is to use the "file analysis" function. This works as today in older versions of IndraWorks.
02-28-2022 11:32 AM
Hello Uwe,
Any Update regarding offline simulation of ctrlx Drive ?
otherwise, any database of .par file to be used in "file analysis" ?
Thanks.
03-01-2022 08:12 AM
Offline simulation like in the past with IndraDrive is still not possible.
For samples of various parameter files have a look to the How-To blogs already available, like: