FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important
information on the platform change.
04-12-2022 09:31 AM
Solved! Go to Solution.
04-26-2022 06:44 AM
In WebIQ the language of the HMI is bound to the user, not globally. We have a UI Action "setlocale (final)" which could be triggered from within a LocalScript when the corresponding item changes. However, changing the locale in WebIQ always forces a reload of the HMI which is probably not what you want as a reload will show the HMI as it looks initially - so if you change the HMI from the outside like this the screen/area where the user was before that change will be lost.
Why would you want to change the language from the PLC in the first place if each WebIQ user can have its own locale?
04-26-2022 08:39 AM
04-26-2022 09:34 AM - last edited on 09-12-2022 04:21 PM by HmiGuide
This is a short example - you can just create a new LocalScript (don't forget to add it to the HMI!) and replace the module.run() code by this block:
module.run = function (self) {
const im = shmi.visuals.session.ItemManager;
const myItemHandler = im.getItemHandler();
myItemHandler.setValue = function (value) {
console.log("The value of the item has been set to " + value);
if (value == 1) {
let p = [{
name: "notify",
params: ["This dialog was triggered by a UI Action!", "UI Action Dialog"]
}];
new shmi.visuals.core.UiAction(p).execute(); // close Dialog
}
};
const subscriptionToken = im.subscribeItem('SInt', myItemHandler);
/* called when this local-script is disabled */
self.onDisable = function () {
self.run = false; /* from original .onDisable function of LocalScript control */
subscriptionToken.unlisten();
};
};
04-26-2022 11:01 PM - last edited on 09-12-2022 04:29 PM by HmiGuide
Just to clarify the previous answer, to call the UI Action associated with language switching, change the name from "notify" to "setlocale" and set params to the appropriate locale string:
See complete script and sample output attached.
A complete listing of UI Actions is given in the documenation here.