FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
12-23-2022 05:20 PM
Hello,
Is there a way to define the local help file by default instead of the Online Help with ctrlX Drive Engineering ?
Thanks!
Solved! Go to Solution.
01-03-2023 08:26 AM
Hello YUL725
What do you mean with "define the local help file by default"?
Currently you have two offline possibilities
Regards
Jochen
01-03-2023 04:56 PM - edited 01-03-2023 04:57 PM
Nice to know.
But another step has to be done. I tried the above mentioned but if I use in a parameter editor window the help it still opens the online help.
You have to activate the following: see screenshot. then the "online"-window opens but with the offline-address.
Regards, Stefan