cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Snaps for ctrlX CORE Virtual RM 20.07

Snaps for ctrlX CORE Virtual RM 20.07

bschmidt
New Contributor

Hello,

Are Motion, PLC, and any other apps available for ctrlX CORE Virtual with RM 20.07? If I try to download the AxisInterface/KinInterface PLC project from the latest ctrlX WORKS of RM 20.07 to the older PLC app from RM 20.04, I get "unresolved external POU references" or similar message that you normally see when the project and and firmware do not match. On the bright side, I copied this example to a real ctrlX CORE project and it is working (after CORE was updated with all the RM 20.07 snaps).

Best regards,

Brian

2 REPLIES 2

Jochen_Mueller
Community Moderator
Community Moderator

Hello Brian

one big point the the RM 20.07:

We have only one app-file for the real/virtual control.

Means you can use the same file to install e.g. motion/PLC/.... either at a real ctrlX or at the virtual ctrlX.

After updating the ctrlX apps you should be able to use the AxisInterface tempalte without error messges....

 

Regards

Jochen

Thanks Jochen, that did work. It didn't work when I tried it previously, but now I realize I was using an old instance of the virtual control. When I made a fresh virtual instance in 20.07, the .app files installed without problem.

Best regards,

Brian

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist