FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
03-20-2024 10:45 AM - edited 03-20-2024 10:49 AM
Hi,
I'm facing an issue where I can only see the 'Python: Current File' option when trying to run my script in the script engine. I've tried reinstalling both the IDE and Python runtime without success. I also tested with IDE versions 118 and 120, but the problem persists. Additionally, the source control tab indicates 'No repository found.'
Has anyone encountered this? How can I run my script in the script engine properly?
Thanks.
Solved! Go to Solution.
03-20-2024 11:19 AM
Is the ctrlX OS - Python Runtime installed? Could you add a system report (how to) so can get some more insights of your system?
03-20-2024 11:25 AM
03-22-2024 06:52 PM
Could you do a test with the current release version 1.20 of the ctrlX OS - IDE app? It can be found in the store area of the collaboration room.
03-25-2024 10:06 AM
03-25-2024 12:32 PM - edited 03-25-2024 12:33 PM
Hi Parco,
regarding the missing entry "Launch Python in Script Engine" you can try two approaches.
Approach 1:
Approach 2:
This error can occur when pressing this control wheel button. You should avoid pressing it. We are investigating the root issue and are planing to fix it in the upcoming release.
------------------------------------------------------------------------------------------------------------------------------------------
In your other attached screenshots you showed two additional topics.
Kind Regards
Daniel