07-04-2023 05:53 AM
It used to works without error and then comes out this warning. Not sure what is this as cannot find the help file.
Solved! Go to Solution.
07-04-2023 07:30 AM
Hello Bobby
we need more information about this issue
Currently it seems that the axis-profile is not called by the scheduler again. Below an example of the scheduler configuration (of my virtual core)... Maybe you can check this settings on your core. Important are the callables under ctrlX Automation..
Regards
Jochen
07-04-2023 07:55 AM
07-04-2023 07:55 AM
Can you please provide your configuration.
07-05-2023 01:49 AM
Which configuration?
07-05-2023 08:03 AM
I think the easiest way would be to generate a system report with active app data and add it here.
07-05-2023 09:06 AM
11-15-2023 12:22 PM
To clarify things:
If yes I guess your scheduler settings are corrupted and needs to be corrected. Please have a look to topic "Motion app hangs in Configuration/Running after booting", there it is mentioned how to reset your scheduler settings.