FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
07-28-2023 12:47 PM
Hello all,
I have a SAFEX-C.12 and I want to activate two semiconductors with OSSD mode, as I want this outputs to be the inputs of the STO of a ctrlX Drive
If I do not activate the OSSD mode then the STO is unlocked and I can drive the ctrlX but after a while the ctrlX Drive gets a F3134 error as their STO inputs are not dinamized,
If I activate the OSSD mode automatically the ctrlX Safety gets an F3810 error and it gets stucked there,
I simplified the program and I tried with another SAFEX and it worked so it seems a HW problem,
What should I do?
Thanks,
Solved! Go to Solution.
07-31-2023 10:45 AM
Hi @ericvergara ,
Regarding this case, could you please provide:
- System info screenshot out of ctrlX Safety Engineering application.
- wiring schematics between SAFEX-C.12 and ctrlX Drive.
Many thanks.
07-31-2023 10:57 AM
Hello @SaDiego
Yes, I attach here the information,
ctrlX Safety Engineering system version:
The wiring between the SAFEX and the Drive looks like this:
The two semiconductors outputs of the Safety are connected directly to the pins 3 and 7 of the XG41 of the drive
Thanks,
07-31-2023 11:43 AM
Thanks @ericvergara .
What I meant with System info is the information taken out of the diagnostics when connected to SAFEX-C.12. Can you please provide?
Regards
07-31-2023 11:49 AM
Sorry 😅
Attach it here
07-31-2023 04:27 PM
08-01-2023 08:15 PM - edited 08-01-2023 08:21 PM
Hello @ericvergara ,
@SaDiego , @M_Mohann , @Marc_S, @Drives_Uwe : FYI
Best regards
Your ctrlX SAFETY Team
08-02-2023 09:27 AM
Hello @AllAutomation
I am sending the Safex back to Service because I have replaced the Safex for another one with the same project and wiring and it works, so seems a HW problem,
Do you have a procedure about how and to who do I need to send the Safex?
Thanks in advance,
08-02-2023 09:06 PM
Hello @ericvergara ,
please send it back to Bosch Rexroth AG - DC-AE/SVC43 - Bgm.-Dr.-Nebel-Str. 2 - 97816 Lohr am Main - Germany.
Please mark it as a complaint (not only repair) to create a quality finding process out of this return.
Best Regards
Your ctrlX SAFETY Team