FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
02-27-2024 07:13 PM
Hello,
On the Diagnostics tab, we have the ability to read CPU Temperature of the SAFEX-C.1x controllers in the most recent software versions. A customer has requested that this parameter be available either readable externally from a PLC for monitoring, or that the CPU temperature can be monitored Inside the Safety program, with the purpose of setting a bit HIGH if the temperature exceeds a pre-defined temperature level.
1. Is the CPU Temperature monitorable from a PLC, either by reading over fieldbus, FSoE or other method?
2. The documentation hints that temperature monitoring is built-in. Does the CPU temperature already trigger a fault/warning/error of some kind, and if so, what is the threshold for this trigger?
3. Is it possible for a customer to set a user-defined temperature threshold for detection in the Safety program?
Solved! Go to Solution.
03-12-2024 02:40 PM
Is the CPU Temperature monitorable from a PLC, either by reading over fieldbus, FSoE or other method?
No the temperature is not available at the PC
2. The documentation hints that temperature monitoring is built-in. Does the CPU temperature already trigger a fault/warning/error of some kind, and if so, what is the threshold for this trigger?
But you get Errornumbers and when this Errors occures you have a temperature problem
3. Is it possible for a customer to set a user-defined temperature threshold for detection in the Safety program?
No this is not possible