FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important
information on the platform change.
02-27-2024 07:13 PM
Hello,
On the Diagnostics tab, we have the ability to read CPU Temperature of the SAFEX-C.1x controllers in the most recent software versions. A customer has requested that this parameter be available either readable externally from a PLC for monitoring, or that the CPU temperature can be monitored Inside the Safety program, with the purpose of setting a bit HIGH if the temperature exceeds a pre-defined temperature level.
1. Is the CPU Temperature monitorable from a PLC, either by reading over fieldbus, FSoE or other method?
2. The documentation hints that temperature monitoring is built-in. Does the CPU temperature already trigger a fault/warning/error of some kind, and if so, what is the threshold for this trigger?
3. Is it possible for a customer to set a user-defined temperature threshold for detection in the Safety program?
Solved! Go to Solution.
03-12-2024 02:40 PM
Is the CPU Temperature monitorable from a PLC, either by reading over fieldbus, FSoE or other method?
No the temperature is not available at the PC
2. The documentation hints that temperature monitoring is built-in. Does the CPU temperature already trigger a fault/warning/error of some kind, and if so, what is the threshold for this trigger?
But you get Errornumbers and when this Errors occures you have a temperature problem
3. Is it possible for a customer to set a user-defined temperature threshold for detection in the Safety program?
No this is not possible