FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
11-08-2022 11:00 AM
Hello! I have CtrlX PLC 1.16 and when I try to use CXA_Datalayer library I always get build error, because it can't find dependent SysTypes library. I can add this library manually and then it's in the libraries list, but in the CXA_Datalayer it's still not resolved and build is not possibel. I've tried reinstallation, it didn't help.
Solved! Go to Solution.
11-11-2022 07:58 AM
Hello OpconUser
I don't have this problem at my 1.16 Installation.
Please can you check if and when what kind of SysTypes is installed at your system.
You can find the lib at the lib-repository.
Regards
Jochen
11-11-2022 02:41 PM
I could solve it and I would like to share the solution:
In the library manager we press "Placeholders" button and then we'll see the following table
Left click on the empty "Library" field next to the "Name" and press the appearing button to choose appropriate library.
After that the library error will disappear.
I have the same version as you have, but somehow the placeholder couldn't find it