FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
08-29-2022 05:17 PM - last edited on 10-08-2022 08:27 AM by MichaelB
When I login the programme,ther have a error:"Unresolved reference:GIVEAPPTORUNTIME"?
What should I do?
Solved! Go to Solution.
08-30-2022 07:49 AM
Hello,
it seems that you try to use motion functionality or only have the CXA_Motion.lib in your library manager but there is no App Motion installed on your system.
So first check if the App Motion is installed on your system.
08-31-2022 02:50 AM
The Motion App is installed on my system.My CxA_Motion Version is 0.4.1.0 and My Motion APP Version is Motion MOT-V-0112.7.
08-31-2022 07:40 AM - edited 08-31-2022 07:42 AM
Could you please try to use the official released version of CXA_MOTION library version "0.4.6.4" coming with ctrlX PLC Engineering "1.12.3" as part of ctrlX WORKS "1.12.9"? It is the one intended to use for ctrlX CORE MOTION app "1.12.7"
08-31-2022 11:33 AM
But now in my PC,I have already installed CtrlXWorks V_0112.2.
If I use ctrlX WORKS 1.12.9,Should I need to remove CtrlXWorks V_0112.2,after then install ctrlX WORKS 1.12.9?
Is it posibile to Upgrade CtrlXWorks V_0112.2 to ctrlX WORKS 1.12.9 ?
What should I dealwith Programme which I write in CtrlXWorks V_0112.2 ?
08-31-2022 12:09 PM
When starting the install routine of ctrlX WORKS you can decide if you want to do a parallel installation or an update of the older one. So both is possible. As your ctrlX CORE as well as your PC software should have the actual release I recommend an update.
When opening a program in CtrlX PLC Engineering that was written in an older version, it asks you if the targets and libraries should get updated. Also here I recommend to do that.