CtrlX PLC Login Error

CtrlX PLC Login Error

Max1
Long-established Member

When I login the programme,ther have a error:"Unresolved reference:GIVEAPPTORUNTIME"?

What should I do?

5 REPLIES 5

Michael_A
New Contributor

Hello,
it seems that you try to use motion functionality or only have the CXA_Motion.lib in your library manager but there is no App Motion installed on your system.
So first check if the App Motion is installed on your system.

Max1
Long-established Member

The Motion App is installed on my system.My CxA_Motion Version is 0.4.1.0 and My Motion APP Version is Motion MOT-V-0112.7.

CodeShepherd
Community Moderator
Community Moderator

Could you please try to use the official released version of CXA_MOTION library version "0.4.6.4" coming with ctrlX PLC Engineering "1.12.3" as part of ctrlX WORKS "1.12.9"? It is the one intended to use for ctrlX CORE MOTION app "1.12.7"

Max1
Long-established Member

But now in my PC,I have already installed CtrlXWorks V_0112.2.

If I use ctrlX WORKS 1.12.9,Should I need to remove CtrlXWorks V_0112.2,after then install  ctrlX WORKS 1.12.9?

Is it posibile to Upgrade CtrlXWorks V_0112.2 to  ctrlX WORKS 1.12.9 ?

What should I dealwith  Programme which I write in CtrlXWorks V_0112.2 ?

CodeShepherd
Community Moderator
Community Moderator

When starting the install routine of ctrlX WORKS you can decide if you want to do a parallel installation or an update of the older one. So both is possible. As your ctrlX CORE as well as your PC software should have the actual release I recommend an update.

When opening a program in CtrlX PLC Engineering that was written in an older version, it asks you if the targets and libraries should get updated. Also here I recommend to do that.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist