Hello,
I have ctrlX DRIVEplus with ctrlX CORE inside and want to try axisinterface. Anybody knows how to do so?
Regards
Babar
Solved! Go to Solution.
The libraries and the template for Axis- and Kin-Interface are included in release RM20.07.1ff. The preliminary documentation (only in german available) is attached here.
There are two ways to start:
1st way: Create a new PLC project and select the template "ctrlX CORE Axis/Kin-Interface". The project includes a "ctrlX COREvirtual" from an older release. At first make an "update device" to actualize the control and switch to a "real" control. Then do a double-click on the device and do the communication settings.
2nd way: use an existing project. Add the libraries CXA_MotionInterface.compiled-library and CXA_MotionInterfaceUser.library to your project. The documentation in the library CXA_MotionInterfaceUser.library includes example code in the program "KinInterfaceUser/_
Examples/Example_KinIfApplicationPart". Or create a new PLC project (like in 1st way) and use Export/Import to get the necessary parts into your program.
See our official documentation https://docs.automation.boschrexroth.com/
For the PLC library CXA_MotionInterface:
"ctrlX PLC Engineering, PLC Libraries, Reference Book --> CXA_MotionInterface"