Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Axisinterface

Axisinterface

Babar
Member

Hello,

I have ctrlX DRIVEplus with ctrlX CORE inside and want to try axisinterface. Anybody knows how to do so?

Regards

Babar 

2 REPLIES 2

Goldfinger
Established Member

The libraries and the template for Axis- and Kin-Interface are included in release RM20.07.1ff. The preliminary documentation (only in german available) is attached here.

There are two ways to start:

1st way: Create a new PLC project and select the template "ctrlX CORE Axis/Kin-Interface". The project includes a "ctrlX COREvirtual" from an older release. At first make an "update device" to actualize the control and switch to a "real" control. Then do a double-click on the device and do the communication settings.

2nd way: use an existing project. Add the libraries CXA_MotionInterface.compiled-library and CXA_MotionInterfaceUser.library to your project. The documentation in the library CXA_MotionInterfaceUser.library includes example code in the program "KinInterfaceUser/_
Examples/Example_KinIfApplicationPart". Or create a new PLC project (like in 1st way) and use Export/Import to get the necessary parts into your program.

 

See our official documentation https://docs.automation.boschrexroth.com/

For the PLC library CXA_MotionInterface:
"ctrlX PLC Engineering, PLC Libraries, Reference Book  -->  CXA_MotionInterface"

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist