FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
05-28-2024 07:41 AM
Hi Community,
I am new in using ctrlX IO XI522001 RS485 Serial Comm, i cant find much information about this module.
Has anyone tried it with PLC program example?
Warmest regards,
Solved! Go to Solution.
05-28-2024 08:38 AM
allo,
you can use the function block for the communication module.
In the library is also an example program available.
The communication parameters are CoE parameters. You find this in the CoE part of the module:
The documetation is at the moment not finish.
Regards
05-31-2024 09:09 AM
06-03-2024 12:58 PM
Hallo Open,
here the wiring for RS485
And here the wirinh for RS422
Regards,
06-07-2024 11:23 AM
Does this ctrlX IO XI522001 module support ModbusRTU (RS485)?
06-07-2024 11:29 AM
Hallo,
yes this module support ModbusRTU. There is a library for the ModbusRTU communication available.
06-10-2024 02:54 AM
Hi @Sozu ,
The ModbusRTU (RS485) communication PLC library, can i use the how to's method CXA_MODBUSRTU library?https://developer.community.boschrexroth.com/t5/Store-and-How-to/Various-methods-to-use-ModbusRTU-RS...
06-10-2024 07:27 AM
Hallo,
you need a special library for the ctrlX IO module. I organise the appropriate library for you.
Regards
06-10-2024 09:13 AM - edited 06-10-2024 09:14 AM
06-18-2024 09:59 AM
Thanks Everyone for reply!
I finally got it working!!! 🙂