cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

ctrlX IO XI522001 Serial Comm example

ctrlX IO XI522001 Serial Comm example

Open
Occasional Contributor

Hi Community,

I am new in using ctrlX IO XI522001 RS485 Serial Comm, i cant find much information about this module.

Has anyone tried it with PLC program example?

Open_1-1716874821875.png

Warmest regards,

9 REPLIES 9

Sozu
Community Moderator
Community Moderator

allo,

you can use the function block for the communication module.

Sozu_0-1716878026686.png

In the library is also an example program available.

The communication parameters are CoE parameters. You find this in the CoE part of the module:

Sozu_1-1716878191140.png

 

The documetation is at the moment not finish.

Regards

 

 

Open
Occasional Contributor

Hi @Sozu ,

Thank you for your reply! do you also have the wiring diagram example?

Warmest regards,

Sozu
Community Moderator
Community Moderator

Hallo Open,

here the wiring for RS485

Sozu_0-1717412240811.png

 

And here the wirinh for RS422

Sozu_1-1717412291511.png

Regards,

Open
Occasional Contributor

Does this ctrlX IO XI522001 module support ModbusRTU (RS485)?

Sozu
Community Moderator
Community Moderator

Hallo,

yes this module support ModbusRTU. There is a library for the ModbusRTU communication available.

 

Open
Occasional Contributor

Hi @Sozu ,

The ModbusRTU (RS485) communication PLC library, can i use the how to's method CXA_MODBUSRTU library?https://developer.community.boschrexroth.com/t5/Store-and-How-to/Various-methods-to-use-ModbusRTU-RS...

Sozu
Community Moderator
Community Moderator

Hallo,

you need a special library for the ctrlX IO module. I organise the appropriate library for you.

Regards

cc2go
Occasional Contributor

I attached you the official version 1.20.10.0, which will be included in next v1.20 Patch and v2.6 Patch.

Example and Docu is within the Lib, you can see in with the library manager

Open
Occasional Contributor

Thanks Everyone for reply!

I finally got it working!!! 🙂

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist