08-19-2021 12:50 PM
Hello community,
I tried to connect my ctrlX Drive (XMS1) to the ctrlX Core. I used the HowTo from CodeKnecht and the YouTube Video from ctrlX DevelopR. But the ctrlX Drive can't be found in the IO Engineering App (Picture below).
Anyone has an idea for a solution? What are typical mistakes in that case?
Greetings
Yannic
Solved! Go to Solution.
08-19-2021 01:20 PM
Please check if your EtherCat master instance is already created on the ctrlX CORE.
Also check if the ctrlX DRIVE communication is set to EtherCat.
08-19-2021 01:34 PM
My EtherCat master instance is created. But how can I check if the ctrlX DRIVE communication is set to EtherCat?
08-19-2021 01:47 PM
And if I try to open IO Engineering from ctrlX Core Webinterface it starts loading something, but it never ends (picture below). If I stop that, the IO Engineering opens, but with no successful search for EtherCAT devices.
08-23-2021 10:39 AM
Please also first check your cable connections: ctrlX CORE out = XF50 and ctrlX DRIVE in = XF21.
Have a look in the how to collection in the drive section how to generally connect your PC to a ctrlX DRIVE. To check the communication setting connect via the additional display or directly connect your PC to port XF20 and try to connect there.
08-24-2021 11:57 AM
Hello,
my solution was directly connect to the ctrlX Drive with Drive Engineering. There I changed the communication from sercos to EtherCAT.