FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important
information on the platform change.
10-18-2024 07:16 PM
Hello there,
I am trying to get Drive AF signal from Onboard Output on Drive. I have 6 DI and 1 DO. I did found one function named Axis state machine: Status word, axis (0x2802:02 / P-0-0115 / --). But, it use two bit(15/14) to get a signal. Do you have any other way around to get AF signal using one Digital output?
We want to connect small led to digital output to get indication showing drive have torque. I do not have any additional IO on drive.
I have attached some snap shot for your reference. Thank you in advance.
10-22-2024 02:17 AM
Might work, but maybe try using the following bit to tell you when its in AF.
If not that, maybe see if bit 8 turns on when you are enabled in the operating mode you want to be in.
10-22-2024 09:00 AM
Correct, use Bit 3 of parameter P-0-0115 to indicate if drive is enabled and following the command value.