05-12-2020 04:41 PM
The functional packages ML, MA, TF will not be available, correct?
Solved! Go to Solution.
05-14-2020 10:56 AM
Yes, they will no longer be available as you are used to from the past.
05-14-2020 11:38 AM
But function wise they will be available again in a similar way:
- pre-configured ready-made functions from Bosch Rexroth
- programming of OEM based functions (on own OEM base)
- programming of OEM based functions in including Bosch Rexroth libraries
- PLC programming based on IEC 61131
09-12-2022 02:29 PM - edited 09-12-2022 02:31 PM
Hello Uwe,
In addition from this topic.
A function as 'Axis error correction' in the SRV → Functional package "Servo function" in the Indradrive.
For the ctrlX drive: will that be a Runtime-option, or must the Core do the job? And if the Core has to do the job, will that work if I use a thirth party EtherCat Master ( Beckhoff Operating modus: Cyclic Position Control)
Regards Johs Heijmink
09-13-2022 08:50 AM
With ctrlX DRIVE there is now only the so called "productivity" package available. This is an option. The today functions are the following:
Mind that you can activate only in summary 8 so called performance points as shown in the screen shots before.