Functional package with ctrlX Drive

Functional package with ctrlX Drive

Toadwart
Member

The functional packages ML, MA, TF will not be available, correct?

4 REPLIES 4

smc
Member

Yes, they will no longer be available as you are used to from the past.

Drives_Uwe
Community Moderator
Community Moderator

But function wise they will be available again in a similar way:

- pre-configured ready-made functions from Bosch Rexroth
- programming of OEM based functions (on own OEM base)
- programming of OEM based functions in including Bosch Rexroth libraries
- PLC programming based on IEC 61131

JohsH
Established Member

Hello Uwe,

 

In addition from this topic.

A function as 'Axis error correction' in the SRV → Functional package "Servo function"  in the Indradrive.  

For the ctrlX drive: will that be a Runtime-option, or must the Core do the job? And if the Core has to do the job, will that work if I use a thirth party EtherCat Master ( Beckhoff Operating modus: Cyclic Position Control)

 

Regards Johs Heijmink

Drives_Uwe
Community Moderator
Community Moderator

With ctrlX DRIVE there is now only the so called "productivity" package available. This is an option. The today functions are the following:

Drives_Uwe_0-1663050548911.png

Drives_Uwe_1-1663051490496.png

Mind that you can activate only in summary 8 so called performance points as shown in the screen shots before.

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist