FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
07-20-2020 01:26 PM - edited 07-21-2020 09:26 AM
Will be a extended I/O interface option (like the DA option for IndraDrive Cs) also available for ctrlX DRIVE?
Solved! Go to Solution.
07-20-2020 01:31 PM - edited 07-21-2020 09:26 AM
04-01-2021 07:01 PM
Hello,
I received the following question: Will it be possible to have both the onboard Drive I/O (DA option) as well as STO once available on the ctrlX DRIVE?
I beleive the answer is "Yes" since STO is always on board and is not an option that can be removed. I do not see how we could get the DA option without STO but would like confirmaton that this is correct.
Thank you.
04-06-2021 08:13 AM
Yes, your assumption is correct. The extended I/O interface is available both for ctrlX DRIVE equipped either with Safe Torque OFF (STO) or Safe Motion (SMO).
Mind as well that from April 2021 on this extended I/O interface is available for first customers prior to release of particular customers from product management.
04-06-2021 08:13 AM
Mind as well that from April 2021 on this extended I/O interface is available for first customers prior to release of particular customers from product management.
01-12-2022 05:33 PM
what´s the exactly amount and specification of DA dig. and analogue IN/Outputs? is it the same than DA at Indradrive before?
01-13-2022 08:08 AM
The DA option incorporates:
- 3 analog Inputs
- 2 analog Outputs
- 8 digital Inputs and Outputs (each 2 of those can be re-parameterized as Outputs/Inputs)