Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Extended I/O interface for ctrlX DRIVE

Extended I/O interface for ctrlX DRIVE

Mr_SafeMotion
Community Moderator
Community Moderator

Will be a extended I/O interface option (like the DA option for IndraDrive Cs) also available for ctrlX DRIVE?

6 REPLIES 6

Mr_SafeMotion
Community Moderator
Community Moderator

Yes, for ctrlX DRIVE a digital/analog extension option is also planned!

Hello,

I received the following question: Will it be possible to have both the onboard Drive I/O (DA option) as well as STO once available on the ctrlX DRIVE?

I beleive the answer is "Yes" since STO is always on board and is not an option that can be removed. I do not see how we could get the DA option without STO but would like confirmaton that this is correct. 

Thank you. 

Yes, your assumption is correct. The extended I/O interface is available both for ctrlX DRIVE equipped either with Safe Torque OFF (STO) or Safe Motion (SMO).

Mind as well that from April 2021 on this extended I/O interface is available for first customers prior to release of particular customers from product management.

Mind as well that from April 2021 on this extended I/O interface is available for first customers prior to release of particular customers from product management.

Fred1
Occasional Visitor

what´s the exactly amount and specification of DA  dig. and analogue IN/Outputs? is it the same than DA at Indradrive before?

Drives_Uwe
Community Moderator
Community Moderator

The DA option incorporates:

- 3 analog Inputs
- 2 analog Outputs
Drives_Uwe_1-1642057652203.png
- 8 digital Inputs and Outputs (each 2 of those can be re-parameterized as Outputs/Inputs)

Drives_Uwe_0-1642057590419.png

 


                                                                                                                                  

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist