04-19-2023 10:51 PM - edited 04-19-2023 10:55 PM
I was working with the smart function kit for handling version 2.0.2. I upgraded to 2.5.0 and now have the error that the axis is not referenced while it is referenced. How can I resolve this?
Solved! Go to Solution.
04-21-2023 09:24 AM
Hello aFouraker,
please make sure that all drives have a reference.
If this does not help you could manually set the reference with a ctrlX DataLayer Command.
For this go to the ctrlX HMI and in Settings -> Datalayer (see Screenshot).
Open the Path "smartfunctionkit/communication/cmd/setreference" and click on "Create".
As Input use the Object: {"offset_x": 0,"offset_y": 0,"offset_z": 0}
06-22-2023 04:34 PM
I did try this and it did not change the state. I ended up recommissioning the system.