FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
04-19-2023 10:34 AM
Dear all,
I would like to ask if anyone has ever established a communication between 2 or more ctrlX core units, via sim card 5G gateway.
Let me be more specific:
1. Can data be exchanged between different units using third-party gateways?
2. Can I use node red s/w to view real-time data and send commands to a remote ctrlX core unit via 5G communication? (Like a SCADA system). For example to set the status of a solenoid valve? And what if I want to communicate with 30 different ctrlX core units?
Thank you in advance!
Solved! Go to Solution.
04-21-2023 08:47 AM
We already had some test cases for fairs so in general it is working. We were e.g. using hardware from Nokia.
For your questions:
We suggest using ctrlX CORE - OPC UA Pub/Sub App (based on UDP) for communication between several ctrlX CORE (C2C) in a fast way. See an example here.
04-21-2023 03:59 PM - edited 04-21-2023 04:02 PM
Dear shepherd,
Thank you very much for your reply! I have attached a picture that describes exactly what I want to do...
Stations A & B do not have internet access via ethernet cables. Therefore I have to use 5G sim card modem-routers.
What s/w applications do I need to install on CtrlX CORE units and on the main computer in the control room, to:
1. have an HMI screen in the control room, showing values from all connected CtrlX CORE units? (Can I design scada screens with visuals like tanks, valves, engines, etc.?
2. have remote control of ctrlX CORE units? (On my HMI screen, for example, I want to draw a button and start a motor connected to ctrlX CORE A by simply pressing it)
3. be able to maintain data loggers? (I believe there is the ability to store in the cloud. What s/w application do I need to query the data I need from the cloud and display it on my HMI screen in a trend view?
Thank you very much in advance for your valurable support!
06-22-2023 11:44 AM
Sorry for the late reply lost track of this issue.
Your use case can be done with different solutions. Our suggested one I mentioned above.
For you questions: