Boot-Duration of real ctrlX Core X3

Boot-Duration of real ctrlX Core X3

JohsH
Established Member

Hello all,

We ran some tests with different ctrlC X3 Cores. Here we measured the boot-up time.

crtlX Core Runtime 1.20.    1 drive connected  :

  • Cold boot: (Core with 15 apps) 2 min 12 sec.
  • EtherCat real-time channel setup and Nodes recognized: 42 sec.
  • Switching drives into OP mode: 7 sec.

Total: 3 min and 1 sec.

For some customers this time is too long.  Are there ways to speed up this action, or does the X7 start up faster? ?

 

Regards Johs Heijmink.

 

8 REPLIES 8

Yacine
Long-established Member

Hello, 

I confirm this feedback where more than 3 minutes (really more ...) is a problem for some customer!.

thanks. 

Filip_K
Established Member

Hello,

I also did some tests but with less amount of apps (about 5) and the starting time on 1.20 firmware was above 2mins. As you said, we also have got some complains about long boot-up time and we are also interested in possible speeding-up this proccess...

CodeShepherd
Community Moderator
Community Moderator

We are following this topic internally but the standard bootup time from my experience currently is 2 - 2:30min. Please keep in mind that the ctrlX CORE is not only a PLC but a complete IPC that needs some time to boot up.

JohsH
Established Member

I know the ctrlX Core has some more than only a PLC. We did several timig test ( with several hardware and software) and about 3 minutes is the average. Still my question is open: will the X7 do the bootup faster?

I have also received complaints from potential customers about the boot-up time of the core X3. We also setup a system using 3 instancesof WebIQ runtimes, and found that the boot-up time was extended even further, closer to 5 minutes.

Whether this is really an issue in the field I sort of doubt, as highly automated equipment often takes long periods of time to recover. What I can say for sure is for a simple machine, taking 2-3 minutes to boot up and operate is definitely not ideal.

JHU1XI1
Long-established Member

I also encountered the same problem, the customer Siemens (S7-1500) started quickly, and ctrlx took 3 minutes.

The customer is using 40 of our CTRLX and is very troubled by slow startup.

2023-03-11_21h55_14.png

redford
Long-established Member

@CodeShepherd is there any update regarding this issue with X3 with 2.6 firmware? A big OEM customer of us is also complaining about this. 

@redford:

I've made a quick test with a core X3 and version 2.6.1 and two drives (doubleaxis). Installed apps: Ethercat, Motion, OPC-UA, PLC, 3D-Viewer, WebIQ.

  • Boot time until reachable via Web-UI: 1min 30 sec
  • Time until ethercat is in OP:   2min

I think it is worth if you made a test with your settings and the version 2.6... (now available at the collaboration room)

Regards

Jochen

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist