WebIQ Trend does not plot points. Moves vertically as a horizontal line.

WebIQ Trend does not plot points. Moves vertically as a horizontal line.

AndreasAA
New Poster

I have set up a trend and it is receiving the values. The problem is that the plot is a horizontal line that moves vertically. It seems like it is not storing the previous values. 

Is there a setting I'm missing?

 

1 REPLY 1

webiq-sk
Frequent Contributor

With the provided information it's impossible to answer this.
However, as it looks like you have a text display next to it - does that display change when the value changes? What we have to do here to analyze this:
1. Is the item actually connected correctly and does it change when the source changes?
2. When the source (i.e. OPC-UA server) changes the value can you see that change in UA Expert as well? If not, the OPC-UA server has probably not been setup correctly.

Please provide the log file and the HMI for analysis.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist