FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
03-25-2023 07:57 PM
I have set up a trend and it is receiving the values. The problem is that the plot is a horizontal line that moves vertically. It seems like it is not storing the previous values.
Is there a setting I'm missing?
Solved! Go to Solution.
03-27-2023 08:11 AM
With the provided information it's impossible to answer this.
However, as it looks like you have a text display next to it - does that display change when the value changes? What we have to do here to analyze this:
1. Is the item actually connected correctly and does it change when the source changes?
2. When the source (i.e. OPC-UA server) changes the value can you see that change in UA Expert as well? If not, the OPC-UA server has probably not been setup correctly.
Please provide the log file and the HMI for analysis.