12-06-2023 12:47 PM
I have a WebIQ application running on CtrlX Core.
Ctrlx App Release V1.20.
WebIQ Server App 2.14.3.
Sometimes the WebIQ application becomes unreachable.
I can't find any messages in the Logbook.
Trying to open WebIQ Runtime Manager I get the error ERR_CONNECTION_TIMED_OUT.
Can anyone help me understand the cause of the problem and fix it?
12-06-2023 03:14 PM
Hi @alnapi ,
If you reboot, the CORE can you access the runtime manager? If so, could you please download and post the logs under Settings-->Log Settings at the bottom of the page?
There is a known incompatability with ctrlX V1.20 and WebIQ V2.13, but this was fixed in V2.14. The versions listed should be compatible.
12-06-2023 03:48 PM
Hi @Sgilk,
I confirm, if I reboot the control I can reach the runtime manager.
Unfortunately, before restarting, I did not proceed to download the log in CSV format. I'll do it next time.
In the meantime, I will try to install the version you recommend: I use the conditional because the machine is already in production.
12-06-2023 03:50 PM
Moved to corresponding sub forum Smart HMI - WebIQ Designer and Server.
12-06-2023 03:56 PM
I meant that the versions you specified should be compatible. There should be no need to change versions, however there is a new major version of 2.15 released at this point.
12-06-2023 04:07 PM
Please note that there was an issue that was presumed to be fixed but it wasn't as it looks until WebIQ 2.15.6 which will hopefully be released soon for ctrlX. I cannot give you any timing on this, because it's currently in Bosch Rexroth testing.
12-06-2023 04:10 PM
If someone needs the version 2.15.6 of the WebIQ server for ctrlX CORE feel free to send me a private message with your contact data so we can share it with you.
12-11-2023 10:24 AM
2.15.6 is now available in the ctrlX store