06-06-2024 03:24 PM - edited 06-06-2024 03:33 PM
Hello all
New CtrlX user here!
Has anybody had any experience with installing community-contributed plugin on the official Telegraf app?
I'm using version 2.4.0+1.28.2 of Telegraf
Best regards,
Michael
Solved! Go to Solution.
06-06-2024 07:45 PM - edited 06-06-2024 08:01 PM
Hi @MichaelEjigu ,
Unfortunately, installation of community-contributed or any plugin not included with the built snap is not supported. The plugins must be included during the compilation process. If you'd like to install a non-supported plugin, you will need to build from source. The list of included plugins can be found here: ctrlX Telegraf Plugins
That being said, there are a large number of plugins included with the current build. Here is a snippet from the Telegraf diagnostic logs.
Available plugins: 241 inputs, 9 aggregators, 30 processors, 24 parsers, 60 outputs, 6 secret-stores
Here is an example configuration utilizing the MQTT output and the ctrlX datalayer input plugins.
[[outputs.mqtt]]
servers = ["192.168.1.200:1883"]
username = "sgilk"
password = "sgilk"
insecure_skip_verify = false
topic = 'telegraf/{{ .PluginName}}/{{ .Tag "measurement"}}'
layout = "field"
## Configure the input plugin with the username and password to ctrlX Core
[[inputs.ctrlx_datalayer]]
## Hostname or IP address of ctrlX CORE
server = "localhost"
## Authentication credentials
username = "boschrexroth"
password = "boschrexroth"
## Use TLS but skip chain & host verification
insecure_skip_verify = true
[[inputs.ctrlx_datalayer.subscription]]
## The name of the measurement. (default: "ctrlx")
measurement = "metrics"
nodes=[
{name="cpu_usage_percent", address="framework/metrics/system/cpu-utilisation-percent"}
]
06-07-2024 11:40 AM
Thank you for your feedback, I will check out the listed plugins and maybe create a feature request (once I find out how) if the pre-included plugins are not sufficient. Being able to integrate plugins as a user would also allow to update plugins at a faster rate than the official app updates.
I am not familiar enough with telegraf yet to judge if this is even technically feasible
I will accept your reply as a solution once i have figured out how to create a feature request
Thanks again
06-07-2024 03:42 PM
The technical problem is that Telegraf is written in Go and compiles to a single binary. To execute this in ctrlX OS, it must be packaged as an Ubuntu snap. If a plugin needs to be added, the Telegraf source must be recompiled and packaged as a new snap.
The good news is that Telegraf (and the ctrlX fork) is open source. You can take this, add your custom plugin, recompile and package as a custom snap to install on the ctrlX OS system.
06-07-2024 03:45 PM
Great!
Thanks again
Michael