Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

ctrlX EoE communication to Elmo drive not working

ctrlX EoE communication to Elmo drive not working

Open
Occasional Contributor

Hi Community,

I am trying to establish connection to Elmo Drive via EoE, but it is not working.

EtherCAT Master:

Open_0-1726543529367.png

Open_1-1726543560883.png

Open_2-1726543614751.png

Enabled IP Forwarding:

Open_0-1726544067408.png

Open_1-1726544095413.png

Command Prompt ping successful:

Open_3-1726543698794.png

Elmo Application Studio:

Open_1-1726723896642.png

Open_2-1726723931418.png

Anyone have success connecting into Elmo drive?

Warmest regards,

2 REPLIES 2

Open
Occasional Contributor

Anyone had success EoE connection from the ctrlX to Elmo drive via Elmo Application Studio III? 

I managed to ping the Elmo drive but unable to connect in the Elmo Application Studio.

Warmest regards,

CodeWasi
Occasional Contributor

Hello ,
checked the setup of EOE with a HarmonicDrive und a ctrlX.
Enable the IP Forwarding on XF10 and EoE like you show in your screens. 
ctrlX-IO Setup done like you did. 
Please consider to test the EAS connection running ECAT_EoE_TCP/IP protocol. I am not that familiar with the dos and donts... but the EAS relies on cyclic and fast communication with ms. I assume your ECAT operates as well with 2ms, right? I did not find a adjustment for the Mailbox-settings and left it default.
Find the figures below:

  1. EAS : File/Settings:
  2. EOE Routing (consider to 255.255.255.0)
  3. Destination: _._._.0 Network-number; Gateway:  IPctrlX   
  4. Target the EAS wants to communicate:  
  5. Check the IP Forwarding.

 

CodeWasi_0-1727790551410.png

If the setup will not succeed - please consider return with Elmo-Drive-FW-infos.

Bye 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist