FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
09-17-2024 05:31 AM - edited 09-19-2024 07:32 AM
Hi Community,
I am trying to establish connection to Elmo Drive via EoE, but it is not working.
EtherCAT Master:
Enabled IP Forwarding:
Command Prompt ping successful:
Elmo Application Studio:
Anyone have success connecting into Elmo drive?
Warmest regards,
Solved! Go to Solution.
09-19-2024 04:56 AM - edited 09-19-2024 04:58 AM
Anyone had success EoE connection from the ctrlX to Elmo drive via Elmo Application Studio III?
I managed to ping the Elmo drive but unable to connect in the Elmo Application Studio.
Warmest regards,
10-01-2024 03:52 PM
Hello ,
checked the setup of EOE with a HarmonicDrive und a ctrlX.
Enable the IP Forwarding on XF10 and EoE like you show in your screens.
ctrlX-IO Setup done like you did.
Please consider to test the EAS connection running ECAT_EoE_TCP/IP protocol. I am not that familiar with the dos and donts... but the EAS relies on cyclic and fast communication with ms. I assume your ECAT operates as well with 2ms, right? I did not find a adjustment for the Mailbox-settings and left it default.
Find the figures below:
If the setup will not succeed - please consider return with Elmo-Drive-FW-infos.
Bye