FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
04-04-2024 01:00 PM
i trying to install ctrlx-works-2.4.1 but error msg appear "invalid class" how can i resolve this issue
thank you
04-04-2024 01:45 PM
Could you add a full screen picture of the error? At which part of the installation Process does is occur?
04-04-2024 02:01 PM
04-15-2024 08:48 AM
Hello gyoussef,
Maybe your WMI is corrupt, then this may be helpful:
Run in an elevated cmd the command window: winmgmt /salvagerepository
Then execute the command: winmgmt /verifyrepository
to see if it now comes back as consistent.
Regards Oliver
04-15-2024 02:26 PM - edited 04-15-2024 02:34 PM
I have had the same error message during starting the ctrlX WORKS installation exe (here version 2.4.1). Additional I could not start existing virtual cores.
To get it running again I made this sequence at the cmd prompt (adim):
I found this sequence at https://learn.microsoft.com/en-us/answers/questions/684166/failed-to-initialize-all-required-wmi-cla...
I know that the sequence I have done was not complete the sequence which was descriped in the link. But I got some error messages at the other comands. So I only made the fewe lines I have descriped and it works.
Regards
Jochen