FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
11-08-2023 02:51 PM - edited 11-10-2023 11:41 AM
Hi
The system is 8 CtrlX drives (FWA-XD1-AXS-V-0308N-NN.03 | XMS2-W0006ANN-01AETT0NNNN) with Profinet as master communication and at simens PLC as Profinet Master.
scan drives from CtrlX drive engineering (CtrlX WORKS WRK-V-0120) then the list of drives are random sorted. I wil ask for screen dump.
11-08-2023 03:24 PM - edited 11-08-2023 03:24 PM
Do I guess right that you are using a CODESYS communication extension as Profinet master? Moved the topic to the corresponding dub forum "CODESYS - PLC Add-ons".
Could you add at least add a screenshot of what behaviour you are encountering and tell us the versions of the used apps and CODESYS addon?
11-10-2023 11:45 AM
No - only single drives with profinet interface and no Corr. I send a screendump when I get it.
11-13-2023 12:51 PM
11-16-2023 10:33 AM
So to clarify:
ctrlX DIRVE is set to ProfiNet fieldbus communication and all connected to a ProfiNet master controller.
Where is you PC connected to in this scenario? Is there some routing via the control?
Which order is expected by your side?
11-16-2023 11:09 AM
The PC is connected via a switch on the ProfiNet network.
as the first - that the sequence is the same every time and does not change.
But otherwise IP address or name
a month ago
So just to wrap this up, there is no communication issue or similar. Only the sorting in the ctrlX DRIVE Engineering is changing and so confusing in your opinion. I will ask for the reason and see if it can be changed.