Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 

Scan drives with profinet master communication

Scan drives with profinet master communication

POUL
Established Member

Hi

The system is 8 CtrlX drives (FWA-XD1-AXS-V-0308N-NN.03 | XMS2-W0006ANN-01AETT0NNNN) with Profinet as master communication and at simens PLC as Profinet Master.

scan drives from CtrlX drive engineering (CtrlX WORKS WRK-V-0120) then the list of drives are random sorted. I wil ask for screen dump.

6 REPLIES 6

CodeShepherd
Community Moderator
Community Moderator

Do I guess right that you are using a CODESYS communication extension as Profinet master? Moved the topic to the corresponding dub forum "CODESYS - PLC Add-ons".

Could you add at least add a screenshot of what behaviour you are encountering and tell us the versions of the used apps and CODESYS addon?

POUL
Established Member

No - only single drives with profinet interface and no Corr. I send a screendump when I get it.

POUL
Established Member

POUL_0-1699876232742.png

 

POUL_1-1699876255054.png

 

CodeShepherd
Community Moderator
Community Moderator

So to clarify:

ctrlX DIRVE is set to ProfiNet fieldbus communication and all connected to a ProfiNet master controller.

Where is you PC connected to in this scenario? Is there some routing via the control?

Which order is expected by your side?

POUL
Established Member

POUL_1-1700129349437.png

 

 The PC is connected via a switch on the ProfiNet network.

 

as the first - that the sequence is the same every time and does not change.

But otherwise IP address or name

 

CodeShepherd
Community Moderator
Community Moderator

So just to wrap this up, there is no communication issue or similar. Only the sorting in the ctrlX DRIVE Engineering is changing and so confusing in your opinion. I will ask for the reason and see if it can be changed.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist