FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
11-08-2023 02:51 PM - edited 11-10-2023 11:41 AM
Hi
The system is 8 CtrlX drives (FWA-XD1-AXS-V-0308N-NN.03 | XMS2-W0006ANN-01AETT0NNNN) with Profinet as master communication and at simens PLC as Profinet Master.
scan drives from CtrlX drive engineering (CtrlX WORKS WRK-V-0120) then the list of drives are random sorted. I wil ask for screen dump.
11-08-2023 03:24 PM - edited 11-08-2023 03:24 PM
Do I guess right that you are using a CODESYS communication extension as Profinet master? Moved the topic to the corresponding dub forum "CODESYS - PLC Add-ons".
Could you add at least add a screenshot of what behaviour you are encountering and tell us the versions of the used apps and CODESYS addon?
11-10-2023 11:45 AM
No - only single drives with profinet interface and no Corr. I send a screendump when I get it.
11-13-2023 12:51 PM
11-16-2023 10:33 AM
So to clarify:
ctrlX DIRVE is set to ProfiNet fieldbus communication and all connected to a ProfiNet master controller.
Where is you PC connected to in this scenario? Is there some routing via the control?
Which order is expected by your side?
11-16-2023 11:09 AM
The PC is connected via a switch on the ProfiNet network.
as the first - that the sequence is the same every time and does not change.
But otherwise IP address or name
09-18-2024 07:54 AM
So just to wrap this up, there is no communication issue or similar. Only the sorting in the ctrlX DRIVE Engineering is changing and so confusing in your opinion. I will ask for the reason and see if it can be changed.