FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
02-24-2023 06:59 PM
Any ideas why the other languages are not showing up when I add a POU to a PLC Program? I have reinstalled several times, Repaired several times and nothing seems to help. I have also verified that my IndraWorks v14 and v15 Engineering softwares work as they should and show all available languages. The issue is only showing up in CtrlX PLC Engineering. I was thinking maybe a bad install file so I have downloaded the latest files again and still have the issue. Also had an employee install with same files on his computer and he did not have the issue I have. So I am beginning to wonder if it is a .net issue or something local to my computer. Looking for additional ideas outside of what I have tried above.
Solved! Go to Solution.
02-27-2023 08:53 AM
What is the version number of your ctrlX WORKS installation?
02-27-2023 01:10 PM
I have 1.12.7 and 1.12.10 installs and both result in same thing.
04-06-2023 04:22 PM
Hi,
please add the setup log files here. You can find it here : C:\ProgramData\Rexroth\PackageManager\Logs. So zip the folder and add it here.
kind regards
04-06-2023 08:24 PM
Hi,
Issue I believe has been resolved. The computer I was using during that time had a major windows issue and the system actually failed. I have since had my computer replaced. I have installed all the software and had zero issues. Not sure of the specific cause, but I would say it involved something corrupted or missing on my old computer and localized to it.
Thanks